AXIS#.IL.AINSCALE

Description

AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.AINSCALE sets the analog current scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 0 (analog torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode).

The value entered is the motor current per 10 V of analog input. This value may be either higher or lower than 100%, but the actual analog input will be limited by the application current limit (AXIS#.IL.LIMITN and AXIS#.IL.LIMITP ).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A/V

Range

0.001 to 22.4 A/V

Default Value

0.001 A/V

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

Analog Input

Block Diagram for TorqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Loop